Capture Settings Panel
Configure the desired screen capture settings.
Auto Refresh
Refresh the current screen image from the instrument at the specified time interval. Specify an interval between 1 second and 86,399 seconds (24 hours). To stop the continuous generation of screen images, click the "Stop Auto Refresh" button.
The Auto Refresh feature is not available on the Keysight InfiniiVision 2000 and 3000A X-Series oscilloscopes.